x
earth

CUSTOMIZE YOUR EXPERIENCE

SOFTWARE

DEVICES

Data-driven occupant SERVICE

Based upon real-time data the building turns lights on for your early bird employees automatically. As the employee moves from parking lot and zone to zone, the building dynamically creates safety, security, and energy efficiencies. With time, through advanced machine learning, the building will anticipate the typical early bird employees and create a safer environment as they arrive. Event-driven scenes are based upon possible scenarios, such as an intruder in the lobby, tornado from the south, a fire in the west wing, that all require a very different response. Imagine being in the building for the very first time and knowing you could follow the lighting path to safety.


Dynamic orchestration, not Just AUTOMATION

Every aspect of what makes a workspace a productive one is in need of a dramatic upgrade. For example, window shade automation is more than lowering shades on a sunny day. It is aligning that function with a specific use case. A common use case is the lowering of window shades for your presentation to the CEO of your biggest customer which should not involve figuring out AV controls, should not involve a drawstring, and most definitely not involve flipping switches to get the lighting correct for that presentation you spent weeks creating.


Connectivity options to fit your spaces’ individual needs

The CoreSync Platform is built to work with our hardware, and any other control system or third party application that knows open systems and non-proprietary is best for the customer

Core & Shell

The preferred method of design and construction for commercial office buildings today, especially buildings with multiple tenants.

Firstly, it speeds up the design and build process. Defining the core and shell elements of the building first allows for progress to be made in the design of other portions of the building while the long-lead items of the core and shell can be implemented. Once those elements have been planned, work can proceed without having to wait on the interior details.

source: http://watchdogpm.com/blog/why-core-shell-should-be-on-your-real-estate-project-checklist/

 

fit-out tenant space

The alternative to the core and shell method is to fit-out tenant space with ceilings, flooring, lighting, HVAC, etc. before a tenant occupies the space. However, often times these items are altered to accommodate a tenant’s ideas and requirements for the space. The result is a great deal of wasted time spent altering a space that just had new fittings installed.


integration flexibility for class 1 & 2 technologies

CLASS 1 INTEGRATION

The data exchange with the broker. Call it north side. The CoreSync product connects non-IP devices mostly lights but could also be fans, motorized shades, dynamic glass, AV screens etc… to an IP network Call it south side.. any device we put on our IoT platform is Class 1 integrated on the north side.. Other systems may already have an IP/PoE native controller, cameras, door access, HVAC controller etc… these do not need a CoreSync gateway on the south side and if they meet the integration requirements, would be class 1 integrated on the North side.

 

CLASS 2 LEGACY INTEGRATION

Any IP/PoE lighting solution requires a way to get lights powered and communicating on a network all IP/PoE lighting only companies have some sort of gateway/driver solution. Some have combined them and called them nodes, some have tried to imbed them in fixtures to hide them, but the physical components exist.

The CoreSync Platform is supported by our CoreSync team of engineers, ecosystem companies, and our focused advisory representatives.

Request Support